Faults and Messages

A Warning is generally a notification to the user which is not critical and does not require the machine to immediately shut off. A Fault is generally a notification of a critical system failure which will stop machine operation. Depending on the severity of the fault will depend on which system-stop mechanism is used.

Faults and Warnings follow the same pattern and are identified by a four digit code:

G G X X

where GG is a two digit group code, and XX is a two digit ID. All Warnings and Faults have been grouped together so it is easier to identify what part of the system is having trouble.

Group Group #
10 System
11 File
15 Hardware
20 Power
25 Temperature
30 Software
4# Feedback (# indicates feedback number)
50 Motor
55 Wake and Shake
60 Motion
70 FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design
90 Safety

Retrieving Fault and Warning Information

Users can retrieve faults on a per-axis basis with the keyword: AXIS#.FAULTS, where # is the Axis number.

AXIS#.FAULTS will return all faults across all Axes, with the format X-#### where X is the axis number and #### is the four digit fault/warning code.

Retrieving Warnings is very similar, users can use DRV.WARNINGS, or DRV.WARNINGS.

Feedback faults will be returned if the feedback is configured as a feedback source. All feedbacks can be checked for errors regardless if they are configured as a feedback source by checking FB#.FAULTBITS

Clearing Faults/Warnings

Users can clear faults on the drive by using DRV.CLRFAULTS - this will clear faults and warnings at the drive level, for all axes.

Or if desired, AXIS#.CLRFAULTS can be issues and will only clear the faults associated with the specified axis.

The Action Table as well as Hardware Enable can be configured to clear faults as well.

Fault History

Faults are logged to flash memory for convenience and debugging. To retrieve the last 50 faults with timestamps, use the keyword DRV.FAULTHIST.

To retrieve all faults over the lifetime of the drive, use DRV.FAULTHIST /all.

The log can be cleared by issuing DRV.FAULTHISTCLEAR. Note: once cleared, fault history is unrecoverable.

Fault Table

A list of all possible faults and warnings can be found by using the keywords DRV.FAULTLIST and DRV.WARNINGLIST.

Description Cause Remedy
F1000 Firmware and FPGA"Field-Programmable Gate Array" FPGA is a semiconductor device that can be configured by the customer or designer after manufacturing; hence the name "field-programmable" versions are not compatible. The FPGA version does not match the firmware FPGA version constants. Load the FPGA version that is compatible with the firmware.
F1001 Power Board type mismatch detected Power Board image does not match what operational firmware expected Contact customer support to update the drive.
F1002 Power Board Communication fault. Communications with the Power Board Failed AXIS#.CLRFAULTS . If issue persists, contact technical support.
F1003 Power Board FPGA not configured. Communications with the Power Board Failed AXIS#.CLRFAULTS . If issue persists, contact technical support.
F1004 Failed to initialize the system Failure in primary module during software start-up Contact Customer support
F1005 Unrecognized FPGA Fault

Failure within the FPGA Module.

FPGA reported unrecognized fault.

Issue AXIS#.CLRFAULTS , if problem persists contact Customer Support
F1006 FPGA cyclic read fault. Detected a timing issue between the firmware and FPGA. Power cycle the drive. If the fault occurs again, contact Customer Support.
F1007 A Factory MechaWare model failed to load. Failed to read the control loop model from flash. Power cycle the drive. If the fault occurs again, contact Customer Support.
F1100 NV Memory Data (might occur when downloading firmware). Non-volatileinformation is stored in a specific memory to remain accessible even when the application has been powered off memory data is corrupted or invalid. When this fault occurs after a firmware download, it is not an indication of a problem (clear the fault and perform a “save” to the drive). Reset the drive to default memory values using Parameter Load in WorkBench.
F1101 Flash Directory Error File System in unexpected state Download latest firmware, if problems persist, contact Customer Support
F1102 Identity Read Failed EDS information on the drive is not in expected format Contact Customer Support
F1103 Invalid MAC Address The MAC Address stored in the EDS on the drive is invalid Contact Customer Support
F1104 Power Board factory settings file read failed Power Board settings unable to be retrieved Contact Customer Support
F1105 Power Board updateable settings file read failed Power Board settings unable to be loaded Contact Customer Support
F1106 Failure reading Control Board FPGA EDS file Control Board configuration settings unable to be loaded Contact Customer Support
F1107 Power Board Resident FPGA not valid Power Board Resident FPGA not valid Update to latest firmware, if problem persists, contact Customer Support
F1108 Power Board Operational FPGA not valid Power Board Operational FPGA not valid Download latest firmware, if problem persists, contact Customer Support.
F1109 Failure reading Power Board FPGA EDS Failure reading Power Board FPGA EDS Contact Customer Support
F2000 Vbus read is out of thresholds. Hardware problem in bus measurement. Troubleshoot and repair hardware problem.
F2001 Drive Foldback. Maximum drive power has been exceeded. The power has been limited to protect the drive. Motion requires too much power. Change profile to reduce load .
F2002 Output over current. Current exceeds drive peak. Check for short or feedback faults.
F2003 Current sensorA sensor is a type of transducer that converts one type of energy into another for various purposes including measurement or information transfer short circuit. 1. Current sensor short circuit. 2. Motor cable plugged in upside down 1. Restart drive. If issue persists, contact technical support. 2. Plug in cable right-side up.
F2004 Iu current offset limit exceeded. Hardware failure detected. Restart drive. If issue persists, contact technical support.
F2005 Iv current offset limit exceeded. Hardware failure detected. Restart drive. If issue persists, contact technical support.
F2006 Bus over voltage. Bus voltage too high. Usually, this problem is load related. Reduce load or change motion profile. Check system regen capacity; add capacity if needed. Check mains voltage.
F2007 Bus under voltage. Warning issued prior to fault. Bus voltage below threshold value. Check mains voltage.
F2008 Bus capacitor overloaded. Single phase AC input on a drive only rated for three-phase input or excessive single-phase power load. Check mains voltage.
F2009 Regen near capacity, could not prevent over voltage. An F501 Bus Over Voltage has occured while the Regen Resistor was at or above 75% of its dissipation capacity. Increase the size of regen resistor to be able to dissipate more power.
F2010 Regen over power. Too much power stored in regen resistor. Either get larger regen resistor or use DC bus sharing to dissipate power.
F2011 Voltage exceeds motors rating. Drive bus voltage exceeds the motor’s defined voltage rating. Make sure that the motor fits the driving rating.
F2012 Power Stage Fault Power Stage Fault Clear Faults, if problem persists, contact Customer Support
F2013 Regen short circuit. Regen resistor short circuit. Regen IGBT short circuit. Contact technical support.
F2014 Phase loss. Phase loss detected. Check mains power voltage.
F2015 Bus over voltage FPGA. Bus over voltage hard fault. Check mains voltage and check system brake capacity.
F2016 Gate Supply under voltage

Gate Supply under voltage.

Check wiring, if problems persist, contact Customer Support
F2500 Control over temperature sensor 1. High temperature limit reached. Check cabinet ventilation system.
F2501 Power over temperature sensor 1. High temperature limit reached. Check cabinet ventilation system.
F2502 Control under temperature sensor 1. Low temperature limit reached. Check cabinet ventilation system.
F2503 Power under temperature sensor 1. Low temperature limit reached. Check cabinet ventilation system.
F3000 Issue command timed out. Processing a command took longer than the command timeout (10-60 sec depending on the command). Try reducing the CPU load of the drive by deactivating unused features or changing the fieldbus cycle time.
F3001 Negative limit switch triggered. Either a digital input is configured as negative limit switch (DINx.MODE 19) and its state is “off” OR a negative software position limit is configured (AXIS#.SWLS.EN) and the actual position AXIS#.PL.FB is less than the configured limit (see also AXIS#.SWLS.LIMIT# / ). Move the load away from the limits.
F3002 Assert Check Failed Internal Firmware Error Contact Customer Support
F3003 External Fault. This fault is user generated and is caused by user settings. Users can configure a digital input to trigger this fault (DINx.MODE = 10). The fault occurs according to this input setting. Clear the input to clear the fault.
F3004 Operation in Position Mode with Halls Only feedback not allowed. Operation in Position Mode with Halls Only feedback not allowed. Set your drive’s mode of operation to velocity or torqueTorque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist when using a Halls Only feedback.
F4000 Feedback Parity Fault Feedback Parity Fault Check Feedback Settings, if problem persists, Contact Customer Support
F4001 Feedback Overrun Fault Feedback Overrun Fault Check Feedback Settings, if problem persists, Contact Customer Support
F4002 Feedback Framing Fault Feedback Framing Fault Check Feedback Settings, if problem persists, Contact Customer Support
F4003 Feedback CRC"Cyclic redundancy check" A CRC is a type of function that takes as input a data stream of any length and produces as output a value of a certain fixed size. The term CRC is often used to denote either the function or the function's output. A CRC can be used as a checksum to detect accidental alteration of data during transmission or storage Fault Feedback CRC Fault Check Feedback Settings, if problem persists, Contact Customer Support
F4004 Feedback Communication Timeout Fault Feedback Communication Timeout Fault Check Feedback Settings, if problem persists, Contact Customer Support
F4005 Feedback Initialization Sequence Fault Feedback Initialization Sequence Fault Check Feedback Settings, if problem persists, Contact Customer Support
F4006 Feedback Temperature Fault Feedback Temperature Fault Check Feedback Settings, if problem persists, Contact Customer Support
F4007 Feedback battery Fault Feedback battery Fault Check Feedback Settings, if problem persists, Contact Customer Support
F4008 Feedback SensorA sensor is a type of transducer that converts one type of energy into another for various purposes including measurement or information transfer Fault Feedback Sensor Fault Check Feedback Settings, if problem persists, Contact Customer Support
F4009 Feedback DeviceA process whereby some proportion of the output signal of a system is passed (fed back) to the input. In automation, a device coupled to each motor to provide indication of the motor's shaft angle, for use in commutating the motor and controlling its speed and position-Unique Fault 0 Feedback Device-Unique Fault 0 Check Feedback Settings, if problem persists, Contact Customer Support
F4010 Feedback Device-Unique Fault 1 Feedback Device-Unique Fault 1 Check Feedback Settings, if problem persists, Contact Customer Support
F4011 Feedback Analog Signal Fault Feedback Analog Signal Fault Check Feedback Settings, if problem persists, Contact Customer Support
F4012 Feedback Broken Wire Feedback Broken Wire Check Feedback Wiring
F4013 Feedback Power Supply Fault Feedback Power Supply Fault Check Feedback Wiring
F4014 Feedback, Illegal Hall State (111, or 000) Feedback, Illegal Hall State (111, or 000) Check Hall Wiring
F4015 Failed to set feedback type Failed to set feedback type Check Feedback Settings and wiring
F4016 Failed to read motor parameters from feedback deviceA process whereby some proportion of the output signal of a system is passed (fed back) to the input. In automation, a device coupled to each motor to provide indication of the motor's shaft angle, for use in commutating the motor and controlling its speed and position. Motor either does not have motor feedback memory, or the motor feedback memory is not programmed properly so the parameters cannot be read. Try to read parameters again by clicking the Disable and Clear Faults button, or by issuing the AXIS#.CLRFAULTS command. If this attempt is not successful, then set AXIS#.MOTOR.AUTOSET to 0 (off) and program the parameters using the setup wizard or manually set up the parameters. If the motor has motor memory (Biss Analog, Endat, and SFD motors have motor memory), return the motor to have the memory programmed.
F5000 Motor overheated. Motor overheated. Check ambient temperature. Check motor mounting heat sink capability
F5001 Brake 1 Current out of range Brake 1 Current out of range Check Brake Wiring
F5002 Brake 2 Current out of range Brake 2 Current out of range Check Brake Wiring
F5003 Brake applied during Enable-State. Motor brake closed unexpectedly. Check cabling and general functionality.
F5004 Brake released when it should be applied. Brake disengaged unexpectedly. Check cabling and general functionality.
F5005 Drive motor parameters setup incomplete. Before a motor can be enabled, you must configure a minimum set of parameters. These parameters have not been configured. Issue the command AXIS#.SETUPREQLIST to display the list of the parameters that you must configure. Configure these parameters either manually or automatically. You can manually configure these parameters in three ways: (1) set each parameter individually; (2) use the setup wizard to select the motor; or (3) select the motor type from the motor data base in the Motor window (AXIS#.MOTOR.AUTOSET must be set to 0 (off)). If you use the Motor window, you must first select the feedback type. If the motor has Biss Analog, Endat, or SFD feedback (feedback with memory), then these parameters are set automatically when AXIS#.MOTOR.AUTOSET is set to 1 (on).
F5500 Wake and Shake - Insufficient movement There was less movement than defined by AXIS#.WS.DISTMIN . Increase AXIS#.WS.IMAX and/or AXIS#.WS.T . Or try using AXIS#.WS.MODE 1 or 2.
F5501 Wake and Shake - Excess movement AXIS#.WS.DISTMAX has been exceeded in AXIS#.WS.MODE 0. Or more than 360 degrees was traveled in AXIS#.WS.MODE 2. Increase AXIS#.WS.DISTMAX value or reduce AXIS#.WS.IMAX or AXIS#.WS.T . Wake and Shake is not suported for vertical/overhung loads.
F5502 Wake and Shake - Fine-Coarse delta too large. The angle difference between the coarse and fine calculation was larger than 72 deg. Modify AXIS#.WS.IMAX or AXIS#.WS.T and try again.
F5503 Wake and Shake - Over speed AXIS#.WS.VTHRESH was exceeded. Increase AXIS#.WS.VTHRESH value or reduce AXIS#.WS.IMAX or AXIS#.WS.T .
F5504 Wake and Shake - Loop angle delta too large. The angle between complete loops was larger than 72 deg. Modify AXIS#.WS.IMAX or AXIS#.WS.T and try again.
F5505 Wake and Shake - Commutation not initialized. The motor requires the commutation initialization (there are no encoder commutation tracks, Hall sensors, etc.) and no successful Wake and Shake sequence has been performed Clear any faults, activate the Wake and Shake procedure (AXIS#.WS.ARM ) and enable the drive.
F5506 Wake and Shake - Motor U phase missing. No current was detected in the motor's U phase during Wake and Shake initialization (Mode 0 only). Check the motor connections and AXIS#.WS.IMAX (very low current may produce this error).
F5507 Wake and Shake - Motor V phase missing. No current was detected in the motor's V phase during Wake and Shake initialization (Mode 0 only). Check the motor connections and AXIS#.WS.IMAX (very low current may produce this error).
F5508 Wake and Shake - Motor W phase missing. No current was detected in the motor's W phase during Wake and Shake initialization (Mode 0 only). Check the motor connections and AXIS#.WS.IMAX (very low current may produce this error).
F5509 Wake and Shake - Validating Positive Movement Failed. After applying a positive current, motor moved in the wrong direction. Check motor phase wiring and motor encoder wiring is correct.
F5510 Wake and Shake - Validating Negative Movement Failed. After applying a negative current, motor moved in the wrong direction. Check motor phase wiring and motor encoder wiring is correct.
F5511 Wake and Shake - Validating Comm. angle timed out. During one of the W&S validation stages, the drive stopped responding to commands. Contact customer support.
F5512 Wake and Shake - Validating Comm. angle moved too far - Bad Comm Angle. After applying a current, the motor moved too far (>15 electrical degrees). This indicates a poor motor phase angle was found by Wake and Shake. Revise Wake and Shake parameters, and re-run Wake and Shake.
F5513 Wake and Shake - Validating Comm. angle required more than AXIS#.MOTOR.ICONT A current larger than AXIS#.MOTOR.ICONT was used to excite the motor. This indicates one of the following: •Phase angle is incorrect due to a bad wake and shake. •Motor has very high friction requiring high current to break free. •Motor power cable is disconnected or improperly wired.
F6000 Over speed Motor exceeded AXIS#.VL.THRESH Increase AXIS#.VL.THRESH or lower velocity command
F6001 Following error magnitude fault. Motor did not follow command values. Motor exceeded maximum allowed position following error (user). Check feedback commutation setup and tuning parameters.
F6002 Invalid commutation detected - motor accelerating in the wrong direction. Motor phase may be incorrect. The velocity of the motor exceeded AXIS#.WS.CHECKV and the sign of the current was not equal to the sign of motor acceleration or the sign of motor velocity for a period of time larger than AXIS#.WS.CHECKT. 1. Check motor phase wiring 2. Re-configure wake and shake (if Mode 0 or 1 is used) 3. Re-run wake and shake to determine correct commutation angle
F6003 Instability during autotune. Drive current (AXIS#.IL.CMD ) or velocity feedback (AXIS#.VL.FB ) exceeds allowable limit (AXIS#.BODE.IFLIMIT or AXIS#.BODE.VFLIMIT). This fault only occurs in AXIS#.BODE.MODE 5. This fault often occurs when complex mechanics, belts, and compliant loads are present. Change AXIS#.BODE.MODE if appropriate. If AXIS#.BODE.MODE 5 is appropriate and the fault occurs at the end of an Autotuning, then the motor is not robustly stable. You can manually adjust Autotuner settings. Manual tuning may be required to make the motor stable.
F6004 Target position was overshot due to invalid motion task activation. The drive cannot decelerate from its current speed to reach the end point of the second motion task without moving past it. Increase the deceleration rate in the move or trigger the move earlier. Change Motion task profile and clear fault with AXIS#.CLRFAULTS . Or change the value of FAULT139.ACTION = 1 to ignore this condition.
F6005 Emergency timeout occurred. Motor did not stop in the timeout defined in AXIS#.DISTO Change timeout value, change stop parameters, improve tuning.
F6006 Current home mode requires AXIS#.HOME.IPEAK to be set. Some homing modes require AXIS#.HOME.IPEAK to be a non-zero value. Set AXIS#.HOME.IPEAK to a non-zero value or use a different homing mode (AXIS#.HOME.MODE).
F7000 Fieldbus Communication lost. All fieldbus communication was lost. Check fieldbus connections, settings, and control unit.
F7001 Fieldbus Sync frames lost. The fieldbus lost synchronization. Check fieldbus connection, or the settings of your EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs or CANopen master.
F7002 Fieldbus Heartbeat lost. Heartbeat lost. Check CANopen cabling. Reduce bus load or increase the heartbeat update time.
F7003 Fieldbus PLL failed to lock Fieldbus PLL failed to lock Check Fieldbus wiring and settings
F7004 Fieldbus PLL lost lock Fieldbus PLL lost lock Check fieldbus wiring and settings
F7005 Fieldbus cyclic setpoints missing Fieldbus communication interrupted for some reason Check fieldbus wiring and settings
F9000 Safe torque off. Safe torque off function has been triggered. Reapply supply voltage to STO if safe to do so.
F9002 SMM Communication Failed Safe Motion Module not communicating as expected Contact Customer Support
F9003 Incorrect safety card detected Physical SMM module does not match the expected module Contact Customer Support
F9004 Safe torque off pulse and standard lines don't match The two STO inputs did not change state within 100ms of each other. With Pass through: Clear faults With SMM: clear safety IO fault with safe input configured with SAFE.IOERRORACKSOURCE or via FSoE.
F9005 Simultaneity Fault: Safe torque off lines don't match each other Simultaneity Fault: Safe torque off lines don't match each other Contact Customer Support
F9006 SMM in failed state SMM detected a safety I/O failure and faulted. This can be caused by a number of things: digital I/O pulse failed, STO pulse failed, encoder position failure, or serial communication failed. Determine cause and replace necessary hardware if issue reoccurs
F9007 Drive and SMM parameters inconsistent SMM parameters consistency check failed. Contact Customer Support
W1000 Fan stalled. Fan speed is too slow Power Cycle drive, if problem persists Contact Customer Support
W1001 Sync timer PLL. FPGA Synchronization is off Update to latest firmware, if problem persists contact Customer Support
W2001 Drive foldback imminent! Reduce Load. Current command is high enough to trip Drive Foldback threshold soon. Decrease current command by softening tuning gains or a less aggressive motion trajectory. If problem persists, application may require a drive with larger power rating.
W2002 Motor foldback imminent! Reduce Load. Current command is high enough to trip Motor Foldback threshold soon. Decrease current command by softening tuning gains or a less aggressive motion trajectory. If problem persists, application may require a motor with larger power rating.
W2003 Motor I2t load! Reduce load. Current command is high enough to trip Motor I²t threshold soon. Decrease current command by softening tuning gains or a less aggressive motion trajectory. If problem persists, application may require a motor with larger power rating.
W2006 Bus over voltage. Line voltage spiked above VBUS.OVWTHRESH, or motor back emf generated voltage above VBUS.OVWTHRESH. Clear Faults, if problem persists determine source of voltage spike. If problem is power related; power conditioning may be required. If voltage spike is due to motor back-emf, a regen resistor may be required for the application
W2007 Bus under voltage. Bus voltage dipped below VBUS.UVWTHRESH Check supply voltage
W2008 Bus capacitor overloaded. Internal voltage spiked above VBUS.OVWTHRESH, or motor back emf generated voltage above VBUS.OVWTHRESH. Clear Faults, if problem persists determine source of voltage spike. If problem is power related; power conditioning may be required. If voltage spike is due to motor back-emf, a regen resistor may be required for the application
W2010 Regen energy critical. Regen resistor is reaching its capacity Decrease aggressiveness of motion profile, or use larger size regen resistor
W2500 Control Over Temp Sensor 1. Internal control board temperature is overheating Increase air circulation around drive box, check fan operation. If problem persists contact Customer Support
W2501 Power Over Temp Sensor 1. Internal power board temperature is overheating Increase air circulation around drive box, check fan operation. If problem persists contact Customer Support
W2502 Control Under Temp Sensor 1. Internal control board is getting below specified operating temperature Check environment the drive is operating in.
W2503 Power Under Temp Sensor 1. Internal power board is getting below specified operating temperature Check environment the drive is operating in.
W4000 Feedback Parity Warning Feedback Parity Warning Check Feedback Settings, if problem persists, Contact Customer Support
W4001 Feedback Overrun Warning Feedback Overrun Warning Check Feedback Settings, if problem persists, Contact Customer Support
W4002 Feedback Framing Warning Feedback Framing Warning Check Feedback Settings, if problem persists, Contact Customer Support
W4003 Feedback CRC Warning Feedback CRC Warning Check Feedback Settings, if problem persists, Contact Customer Support
W4004 Feedback Communication Timeout Warning Feedback Communication Timeout Warning Check Feedback Settings, if problem persists, Contact Customer Support
W4005 Feedback Initialization Sequence Warning Feedback Initialization Sequence Warning Check Feedback Settings, if problem persists, Contact Customer Support
W4006 Feedback Temperature Warning Feedback Temperature Warning Check Feedback Settings, if problem persists, Contact Customer Support
W4007 Feedback battery Warning Feedback battery Warning Check Feedback Settings, if problem persists, Contact Customer Support
W4008 Feedback Sensor Warning Feedback Sensor Warning Check Feedback Settings, if problem persists, Contact Customer Support
W4009 Feedback Device-Unique Warning 0 Feedback Device-Unique Warning 0 Check Feedback Settings, if problem persists, Contact Customer Support
W4010 Feedback Device-Unique Warning 1 Feedback Device-Unique Warning 1 Check Feedback Settings, if problem persists, Contact Customer Support
W4011 Warning: Gearing feedback source fault. Fault condition was detected on position feedback device referenced by AXIS#.GEAR.FBSOURCE. .
W5000 Motor overheated. Motor overheated. Check ambient temperature. Check motor mounting heat sink capability
W5001 Brake override active Brake override active The parameter AXIS#.MOTOR.BRAKECONTROL overrides actual brake control of the drive.
W5500 Wake and Shake - Over speed AXIS#.WS.VTHRESH was exceeded. Increase AXIS#.WS.VTHRESH value or reduce AXIS#.WS.IMAX or AXIS#.WS.T .
W6000 Velocity limit violation, exceeding max limit. A new target velocity calculated internally due to an exception, and is being limited due to user velocity limit. Activation of any new motion or using of AXIS#.CLRFAULTS will clear the warning. Check motion task target velocity settings and parameters to make sure that the values entered will not exceed the AXIS#.VL.LIMITP and AXIS#.VL.LIMITN setting.
W6001 Following error magnitude fault. Motor did not follow command values. Motor exceeded maximum allowed position following error AXIS#.PL.ERRWTHRESH . Check feedback commutation setup and tuning parameters.
W6002 Fault on FB2 is preventing remote commutation for FB1. Attempt to issue motion task before the axis is homed. Axis must be homed before motion task can start. Change opmode or home axis.
W6003 OPMODE incompatible with CMDSOURCE This warning is generated when the drive is enabled and the gearing command source is selected at the same time as torque or velocity op-mode. Select a different AXIS#.OPMODE and AXIS#.CMDSOURCE combination.
W6004 Zero velocity when using induction sensorless feedback type in torque mode. Zero velocity when using induction sensorless feedback type in torque mode. Check motor wiring and tuning parameters. If problem persists contact Customer Support
W6005 Velocity has been limited commutation speed to less than 600Hz to meet ECCN 3A225 requirements. Motor Velocity has exceeded the allowed commutation speed (599Hz). Refer to ECCN 3A225 Limitations for Induction Motors.
W6006 Positive limit switch triggered. Either a digital input is configured as positive limit switch (DINx.MODE 18) and its state is “off” OR a positive software position limit is configured (AXIS#.SWLS.EN) and the actual position AXIS#.PL.FB is greater than the configured limit (see also AXIS#.SWLS.LIMIT# / ). Move the load away from the limits.
W6007 Negative limit switch triggered. Either a digital input is configured as negative limit switch (DINx.MODE 19) and its state is “off” OR a negative software position limit is configured (AXIS#.SWLS.EN) and the actual position AXIS#.PL.FB is less than the configured limit (see also AXIS#.SWLS.LIMIT# / ). Move the load away from the limits.
W6008 Using derivative of position when using sensorless feedback type in position mode Using derivative of position when using sensorless feedback type in position mode Sensorless operation is not allowed for POSITION MODE - change AXIS#.OPMODE to Velocity Mode
W6009 Following motion failed; check motion parameters. Activation of the following motion task failed due to incompatible parameters, or motion task does not exist. Activation of any new motion or using of AXIS#.CLRFAULTS will clear the warning. Check following motion task settings and parameters to make sure that the values entered will produce a valid motion task.
W6010 Target position crossed due to stop command. The motion task crosses the target position after triggering a AXIS#.STOP command. This situation can happen when processing a change-on-the-fly motion task and triggering a AXIS#.STOP command close to the target position of the currently running motion task. Activation of any new motion or using of AXIS#.CLRFAULTS will clear the warning.
W6011 HomingThe Homing procedure allows, based on a position measurement, to set a position offset to the motor in order to ensure it is physically at the home position index pulse not found. A homing mode with index detection is activated, and index pulse is not detected while moving across the range determined by the hardware limit switches. Activation of any new motion or using of AXIS#.CLRFAULTS will clear the warning.
W6012 Homing reference switch not found. A homing mode with reference switch detection is activated and the reference switch is not detected while moving across the range determined by the hardware limit switches. Activation of any new motion or using ofAXIS#.CLRFAULTS will clear the warning.
W6014 Motion task activation failed. Activation of the motion task failed due to incompatible parameters, or motion task does not exist. This warning can appear upon an AXIS#.MT.MOVE command. Activation of any new motion or using of AXIS#.CLRFAULTS will clear the warning. Check motion task settings and parameters to make sure that the values entered will produce a valid motion task.
W6015 Homing procedure failed. Homing error observed during the operation of homing procedure. Activation of any new motion or using of AXIS#.CLRFAULTS will clear the warning.
W6017 Motion task target position is out. This warning appears with W6014. This warning is triggered when you try to trigger a motion task with an absolute target position outside of the selected modulo range (see also AXIS#.MT.CNTL). Move the absolute target position of the motion task within the modulo range. Activation of any new motion or using of AXIS#.CLRFAULTS will clear the warning.
W6018 Motion task target position is out of software-limits. Motion Task position has passed a software limit switch Review software limit switch configuration and motion task configurations and remove incompatibilities.
W6019 Invalid bit combination in the motion task control word. This warning appears with W6014. This warning is triggered when you try to trigger a motion task with an invalid bit combination in the motion task control word (see also AXIS#.MT.CNTL). Correct the AXIS#.MT.CNTL setting for the specific motion task. Activation of any new motion or using of AXIS#.CLRFAULTS will clear the warning.
W6020 1:1 profile cannot be triggered on the fly. This warning appears with W6014. This warning is triggered when you try to trigger a 1:1 profile table motion task while another motion task is currently running. 1:1 profile table motion tasks should be started from velocity 0. Activation of any new motion or using of AXIS#.CLRFAULTS will clear the warning.
W6021 Customer profile table is not initialized. This warning appears with W6014. This warning is triggered when you try to trigger a motion task that uses a customer profile table for generating the velocity profile and when the selected profile table is empty (see AXIS#.MT.CNTL and MT.TNUM. Change the MT.TNUM parameter for this specific motion task in order to use an initialized profile table. Activation of any new motion or using of AXIS#.CLRFAULTS will clear the warning.
W6022 Motion task activation is currently pending. A motion task tried to execute before the previous task was able to execute Review application timing and allow for adequate time for each motion task to activate before requesting a subsequent motion.
W6023 Homing maximum distance exceeded. Homing maximum distance exceeded. Review tuning and parameter AXIS#.HOME.MAXAXIS#.DIST
W6025 Homing and feedback mismatch. A homing mode is selected which can not work with the current feedback. For example homing modes 3, 6, 10 and 11 all require the feedback to provies a Z / index pulse and not all feedbacks provide this signal. If the homing move is started then it may run continously because it is missing a singnal from the feedback. You will either need to select a different homing mode or change the feedback being used.
W7000 Fieldbus Communication lost. All fieldbus communication was lost. Check fieldbus connections (X11/X12), settings, and control unit.
W7001 Fieldbus Sync frames lost. The fieldbus lost synchronization. Check fieldbus connection or the settings of your fieldbus master.
W9000 Warning: Safe torque off. Safe torque off function has been triggered. Reapply supply voltage to STO if safe to do so.
W9001 Warning: Brake Test Time Overflow A safe brake test has not been executed within the configured time limit Extend safe brake test time limit or execute a safe brake test
W9002 Warning: SMM Over Temperature Safe motion module is over temperature Replace hardware
W9003 Warning: SMM State not operational Safe motion module is not ready to enable. Verify safe id and safe parameters are validated and correct. Check for other faults on the safe motion monitor.
W9004 SMM I/O failure detected SMM I/O failure detected Update to latest firmware, if problems persist, contact Customer Support
W9007 SMM Parameter consistency check fail SMM Parameter consistency check fail Update to latest firmware, if problems persist, contact Customer Support

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen